Motor Temperature View
The motor temperature settings are located in the nested Motor Temperature view.
| Element | Description | Command |
|---|---|---|
| Thermal Resistor Type |
Select the type of thermal resistor.
|
AXIS#.MOTOR.RTYPE |
| Thermal Sensor Source |
Set the source of the thermal sensor. This indicates whether the thermal sensor is connected to the drive through a direct wire connection or through a digital feedback channel.
Devices with a feedback use AXIS#.MOTOR.RSOURCE, while sensorless motors (type 2 or 10) use AXIS#.MOTOR.TEMPSOURCE. |
AXIS#.MOTOR.RSOURCE or AXIS#.MOTOR.TEMPSOURCE |
| Actual Thermistor Value | This field displays the motor temperature, which is represented as the resistance of the motor's PTC or NTC. | AXIS#.MOTOR.TEMP |
| Fault Level |
This field is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensor. A zero value prevents temperature faults from being reported.
|
AXIS#.MOTOR.TEMPFAULT |
| Warning Level |
This field is used to set the motor temperature warning level as a resistance threshold of the motor's PTC. A zero value prevents any warning from being created. |
AXIS#.MOTOR.TEMPWARN |
| Actual Motor Temperature | If the motor has a thermistor with linear characteristics (AXIS#.MOTOR.RTYPE = 2 [KTY83-110], 3 [KTY84-130], 4 [PTC + KTY83-110], or 8 [PT1000]),), this field displays the measured motor temperature in degrees C. For other values of AXIS#.MOTOR.RTYPE this field is hidden. | AXIS#.MOTOR.TEMPC |