VBUS.UVFTHRESH
Description
VBUS.UVFTHRESH sets the undervoltage fault level of the DC bus.
The default value is read from the EEPROM, but can by modified by the user and stored on the NV RAM. This value varies according to drive type.
General Information
|
Type |
R/W Parameter |
|
Units |
VDC |
|
Range |
90 to 420 VDC |
|
Default Value |
90 VDC |
|
Data Type |
Integer |
|
See Also |
VBUS.OVFTHRESH |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| MKD-N | Yes |
| MKD-C | No |
| Index/Subindex | Object Start Version |
|---|---|
|
361Dh/0 |
M_01-00-00-000 |
Related Topics
Regeneration