FBD Corners

Corners are used to force the routing of connection lines, as the FBD editor imposes a default routing only between two pins or user-defined corners.

All variable symbols and constant expressions are entered in FBD diagrams using small boxes.

Select the Insert Corner button in the FBD toolbar to insert a corner on a line:

Insert Corner

In this mode, the mouse is used to insert a user-defined corner on a line.

  • Drag a new line from an output pin to an empty space.
    • In this case, the editor automatically finishes the line with a user-defined corner.
    • Continue drawing the connection to the desired pin and force the routing while you are drawing the line.
  • Corners can then be selected and moved to change the routing of existing lines.