FFLD Data In / Data Out

The data in and data out items are used to either:

  • Initiate a flow (line) with the value of a variable.
  • Force a variable on output with the value of a flow:
    VarIn>- .......... ->VarOut

When used with a block, the data in and data out items can be put close to the block, without any line in-between to connect a variable to an input or output of the block.

Example

The @ symbol in front of the V variable indicates it is used for input and output. (Figure 1)

Figure 1: Input / Output @ Symbol