FFLD Selection Grid

The diagram is entered in a logical grid, and all objects are snapped to the grid.

  • Use the View menu commands to see hiding grid points.
    • This helps locate errors detected by the compiler or aligning objects in the diagram.
  • Zoom in or out of the edited diagram.
  • Drag the separation lines in vertical and horizontal rulers to freely resize the cells of the grid:

       


  • If a split window is in use, the zoom applies only to the currently selected split window (each split window can be zoomed to different levels).

  • The current position in the grid is always highlighted by a dotted cell.
    • Its coordinates (row, column) are displayed at the bottom left-hand corner of the editor.
  • Click the current position, the cell is drawn as gray, meaning that it can be dragged somewhere else in the diagram.
    • Select multiple cells with the mouse, or use the arrows of the keyboard with the <SHIFT> key pressed.
  • Click the power rail (gray ruler at the left border) to select a full row.

These commands are available from the keyboard:

Keys

Description

Arrows

Move focus cell or scroll through ladder.

Ctrl-Shift-F2

Go to previous bookmark.

Ctrl + A

Selects the whole network.

If pressed again, selects the whole program.

Ctrl + F

Performs a Search and Replace (+ add hyperlink on the topic) within the whole program.

Ctrl + Home/End twice

Moves the cursor to the beginning or the end of the program.

Ctrl + Page Up Down

Moves the cursor to previous or next network header.

End

Moves the cursor to the end of the line.

If pressed again, moves the cursor to the end of the network.

Esc / Shift-Esc

Close the rename widget.

Home

Moves the cursor to the left of the line.

If pressed again, moves the cursor to the head of the network.

Page Up / Down

Scroll 1 page.

Return

Equivalent to a double-click.

Shift-Arrow

Multi-select cells.

Shift-Page Up / Down

Selection page up or down.

Shift-Tab

Move focus cell left.

Space

Change contact or coil.

Tab

Move focus cell right.