RAD_TO_DEG

PLCopen motion icon This function/function block was added in KAS v4.04

 Function - Converts a radian value to a degree value.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

LREAL

No range

Radian

No default

Radian value.

Outputs

Output

Data Type

Range

Unit

Description

Q

LREAL

No range

Degree

Degree value equivalent to the radian input.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE. 
    • The output rung (ENO) keeps the same value as the input rung.

IL Language Example

Not available.

ST Language Example

num_degrees := RAD_TO_DEG(num_radians);

See Also

DEG_TO_RAD