Diagnostic Panels - Home page

Usage

This window is used to:

  • View Control Panels designed in the KAS-IDE in a web browser.
  • See Web Diagnostic Panels to enable this feature.

Access

Window Description


  • The content of this window depends on the specific application project controls.

The window shows this information:

  • Connection status with KAS Runtime.
  • Control page zoom setting adjustments.
  • A collapsible side bar with links to view all control panels present in the KAS project.

Notes

  • After a period of inactivity, the Diagnostic Panel session times out and disconnects from the KAS Web server.
    • This is indicated by the message Connection is closed displayed on the top bar. (Figure 1)
    • Figure 3: Diagnostic Panel - Connection closed

  • During this time, widgets in the panel stop refreshing with new data.
    • Text widgets may display a question mark (?) or remain blank.
    • This indicates there is no active connection to the KAS Web server.
  • To restore the connection and update the data, reload the page using the browser’s refresh option.
  • When the KAS project is not running, the top bar shows this message: PLC: Stopped. (Figure 4)
  • Figure 4: Diagnostic Panel - PLC Stopped

  • During this time, widgets in the panels are inactive.
    • Text widgets may show a question mark (?) or remain blank.
  • When the project starts, the status bar and data update automatically.
    • If data does not refresh, reload the page using the browser’s refresh option.

See Also

Diagnostic Panels sub-tab