AXIS#.BODE.CHIRP.STARTFREQ
Description
AXIS#.BODE.CHIRP.STARTFREQ sets the start frequency for the chirp excitation
Example
Setting up a chirp excitation source of 0.2 A from 0.1 Hz to 1000 Hz over a period of 1 second:
--> AXIS1.BODE.INJECTPOINT 1
--> AXIS1.BODE.IAMP 0.2
--> AXIS1.BODE.CHIRP.STARTFREQ 0.1
--> AXIS1.BODE.CHIRP.ENDFREQ 1000
--> AXIS1.BODE.CHIRP.TIME 1
--> AXIS1.BODE.MODE 6
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-04-000 |
General Information
| Type |
Read/Write |
| Description | Sets the start frequency of the chirp excitation. |
| Units | Hz |
| Range | 0.1 to 8,000 Hz |
| Default Value | 0.1 Hz |
| Data Type | Float |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.