AXIS#.BODE.CHIRP.TIME
Description
AXIS#.BODE.CHIRP.TIME sets the duration of the chirp, how long it will take to sweep from the start frequency to the end frequency.
Example
Setting up a chirp excitation source of 0.2 A from 0.1 Hz to 1000 Hz over a period of 1 second:
--> AXIS1.BODE.INJECTPOINT 1
--> AXIS1.BODE.IAMP 0.2
--> AXIS1.BODE.CHIRP.STARTFREQ 0.1
--> AXIS1.BODE.CHIRP.ENDFREQ 1000
--> AXIS1.BODE.CHIRP.TIME 1
--> AXIS1.BODE.MODE 6
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-04-000 |
General Information
| Type |
Read/Write |
| Description | Sets the duration of the chirp excitation. |
| Units | Seconds |
| Range | 0.5 to 10.0 seconds |
| Default Value | 1 Second |
| Data Type | Float |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.