AXIS#.MOTOR.IDMAX

Description

This parameter is supported for IPM motors (AXIS#.MOTOR.TYPE = 6). AXIS#.MOTOR.IDMAX is the maximum motor winding current in the direct (non-torque producing) axis.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 6

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0.2 to 1000

Default Value

0.5 * AXIS#.MOTOR.IPEAK

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.IDMAX

500bh

27h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6232

1

6232 (0x1858)

AXIS1.MOTOR.IDMAX

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTOR.IDMAX

6232

Float

Read Only

-