AXIS#.MOTOR.VOLTRATED

Description

This parameter configures the drive for the induction motor's rated voltage as indicated on the nameplate.

AXIS#.MOTOR.VOLTRATED is used to calculate the constant Volts per Hertz characteristics of the drive and motor.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 2.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

V

Range

50 to 1,000 V

Default Value

230 V

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.VOLTRATED

500bh

06h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6226

1

6226 (0x1852)

AXIS1.MOTOR.VOLTRATED

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTOR.VOLTRATED

6226

Unsigned16

Read/Write

-