AXIS#.PL.ERRWTHRESH

Description

If this value is not equal 0 and the position error AXIS#.PL.ERR is larger than this value, the drive will generate a warning.

If AXIS#.PL.ERRWTHRESH is set to 0 the warning is not issued.

Example

Set position rotary units to 2 degrees. If you set AXIS#.PL.ERRWTHRESH to 100 and the position error is larger than 100 degrees, then the drive will generate a warning.

AXIS#.UNIT.PROTARY 2
AXIS#.PL.ERRWTHRESH 100

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

0 counts

Data Type

Float

See Also

AXIS#.PL.ERR

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.ERRWTHRESH

500ch

02h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5903

1

5903 (0x170f)

AXIS1.PL.ERRWTHRESH

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PL.ERRWTHRESH

5903

Signed32

Read/Write

Position