AXIS#.PL.KFB

Refer to AXIS#.PL.KFB.PIN for details.

Versions

Action Version Notes
Implemented 02-08-00-000  

General Information

Type Read/Write
Units N/A
Range - 2,147,483,648 to 2,147,483,647
Default Value 1.0
Data Type Float
See Also AXIS#.PL.KFB.PIN, AXIS#.PL.KFB.POUT
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.KFB

500ch

0dh

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5927

1

5927 (0x1727)

AXIS1.PL.KFB

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PL.KFB

5927

Float

Read/Write

-