AXIS#.TUNING.QUICKTUNE.START

Description

AXIS#.TUNING.QUICKTUNE.START triggers the execution of the QuickTune procedure and is responsible for taking an inertia measurement of the load and then calculating an ideal target bandwidth. The axis must be enabled for this procedure to run. After the procedure has finished successfully AXIS#.TUNING.BANDWIDTH will be set to either the AXIS#.TUNING.TARGETBANDWIDTH or AXIS#.TUNING.USERBANDWIDTH value and the drive is tuned accordingly.

Versions

Action Version Notes
Implemented 02-12-02-000 

-

General Information

Type Command
Units N/A
Range N/A
Default Value N/A
Data Type N/A
See Also AXIS#.TUNING.BANDWIDTH
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.QUICKTUNE.START

5021h

05h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5042

1

5042 (0x13b2)

AXIS1.TUNING.QUICKTUNE.START

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.TUNING.QUICKTUNE.START

5042

Unsigned8

Read/Write

-