AXIS#.OPMODE
Description
AXIS#.OPMODE specifies the operation mode of the axis. AXIS#.CMDSOURCE must also be used to set the source of the command to the axis.
The operation mode values can be set as follows:
|
Mode |
Description |
|---|---|
|
0 |
Current (torque) operation mode |
|
1 |
Velocity operation mode |
|
2 |
Position operation mode |
AXIS#.OPMODE can be changed while the axis is enabled or disabled. If using the terminal to change the operation mode, it is recommended to disable the axis before changing the operation mode. If changing the operation mode from the terminal while the axis is enabled, the system may experience a step change in demand.
Example
Set the source of the command to a TCP/IP channel and the desired operation mode to velocity:
-->AXIS1.CMDSOURCE 0
-->AXIS1.OPMODE 1
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.OPMODE |
5000h |
05h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5015 |
1 |
5015 (0x1397) |
AXIS1.OPMODE |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.OPMODE |
5015 |
Unsigned8 |
Read/Write |
- |
Related Topics
Gantry Mode