AXIS#.WARNINGS
Description
Indicates what warnings are present on an axis.
Examples
In a scenario where a warning is present on AXIS1, the following output would be seen:
-->AXIS1.WARNINGS 4311: Warning: Gearing feedback source fault.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemente3d | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | String |
| Stored in Non-Volatile Memory | No |
Variants Supported
Supported on all device types.