DRV.CLRFAULTHIST
Description
DRV.CLRFAULTHIST clears the fault history from the non-volatile memory of the drive.
This command erases all faults returned by DRV.FAULTHIST.
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | Yes |
*For PROFINET, write a value of 0 into the PNU to execute a command.