MOTOR.PHASE

Description

This parameter sets the motor phase.


  • If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.


  • When loading a parameter file to a new device, if MOTOR.AUTOSET = 0 then motor parameters should be checked to make sure they are properly configured for the motor on the new device.

General Information

Type

NV Parameter

Units

Electrical degrees

Range

0 to 360°

Default Value

0°

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
359Ch/0 M_01-00-00-000

Related Topics

"Motor View"