AXIS#.PL.KFB.PIN

Description

AXIS#.PL.KFB.PIN and AXIS#.PL.KFB.POUT allow the user to scale the position feedback source into the position control loops.

It is recommended to use AXIS#.PL.KFB.PIN and AXIS#.PL.KFB.POUT instead of AXIS#.PL.KFB due to possible precision loss, however it is not required. For example, the gear ratio 1:3 is precisely represented with the fraction 1/3 but lacks precision as a floating-point number 0.333333.

AXIS#.PL.KFB is related to AXIS#.PL.KFB.PIN/POUT in the following way:

AXIS#.PL.KFB = AXIS#.PL.PIN / AXIS#.PL.POUT.

This gain is especially useful in dual-loop applications where the position loop feedback and velocity loop feedback come from different devices. AXIS#.PL.KFB and AXIS#.VL.KFB can be used to synchronize the values.

Examples

Usage

Do not change from default (1) unless the application is using multiple feedback devices for an axis.

If the situation arose where two feedbacks were mounted to a rotary motor, and one of them was half the resolution of the first - and it was connected to the position feedback, while the full resolution device was connected to the velocity feedback, AXIS#.PL.KFB.PIN would need to be set to 2 and AXIS#.VL.KFB would be left at 1.0

Versions

Action Version Notes
Implemented 02-08-01-000  

General Information

Type Read/Write
Units N/A
Range -2,147,483,648 to 2,147,483,647
Default Value 1
Data Type Integer
See Also AXIS#.PL.KFB, AXIS#.PL.KFB.POUT, AXIS#.VL.KFB
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.KFB.PIN

500ch

11h

Signed32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5918

1

5918 (0x171e)

AXIS1.PL.KFB.PIN

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PL.KFB.PIN

5918

Signed32

Read/Write

-