AXIS#.TUNING.USERBANDWIDTH
Description
AXIS#.TUNING.USERBANDWIDTH is used to override the AXIS#.TUNING.TARGETBANDWIDTH calculated by the QuickTune feature. If this value is non-zero, AXIS#.TUNING.BANDWIDTH will be set to this value on the next QuickTune execution.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-12-02-000 |
- |
General Information
| Type | Read / Write |
| Units | Hz |
| Range | 0.0 to 50.0 |
| Default Value | 0 |
| Data Type | Double |
| See Also | AXIS#.TUNING.QUICKTUNE.START |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.TUNING.USERBANDWIDTH |
5021h |
08h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5047 |
1 |
5047 (0x13b7) |
AXIS1.TUNING.USERBANDWIDTH |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.TUNING.USERBANDWIDTH |
5047 |
Float |
Read/Write |
- |