DIO.STATES

Description

DIO.STATES reads the states of the bi-directional I/Os. Each bit corresponds to a digital state. Bit 0 = DIO1 ... Bit 5 = DIO6.

Examples

Usage

When DIO1 and DIO3 are active (DIO#.STATE = 1). Bits 0 and 2 would be set. DIO.STATES would be 5.

Code

--> DIO.STATES
5

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 63
Default Value N/A
Data Type Integer
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIO.STATES

3680h

00h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2701

1

2701 (0xa8d)

DIO.STATES

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DIO.STATES

2701

Unsigned32

Read Only

-