REC.DONE

Description

REC.DONE indicates that the recorder has finished recording. This value is reset to 0 when the recorder trigger is set. The drive also resets this value when the recording has finished or when REC.OFF is executed.

Examples

Code

Indicates that recording has not completed, either because the triggering has not been completed or that the data capturing is ongoing.

-->REC.DONE
0

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

See Also

REC.ACTIVE , REC.OFF

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2301

1

2301 (0x8fd)

REC.DONE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REC.DONE

2301

Unsigned8

Read Only

-