REC.TRIGPARAM

Description

REC.TRIGPARAM sets the parameter the recorder uses to trigger the capture.

This parameter is not used when REC.TRIGTYPE is 0 (Immediate) or 1 (On Next Command).

The parameters that can be used with REC.TRIGPARAM are listed by REC.TRIGPRMLIST. The parameters that can be used as a trigger also have the [Trigger] tag in their DRV.HELP output.

Example

To set the recorder to trigger on the velocity command signal:

--> REC.TRIGTYPE 2
--> REC.TRIGPARAM VL.CMD

VL.CMD is replaced with AXIS#.VL.CMD for AKD2G.

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

N/A

Default Value

AXIS1.IL.FB (See AXIS#.IL.FB )

Data Type

String

See Also

DRV.HELP , REC.TRIGPRMLIST, REC.TRIGTYPE

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2320

1

2320 (0x910)

REC.TRIGPARAM

String

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

REC.TRIGPARAM

2320

String

Read/Write

-