REGEN.POWER

Description

This parameter reads regen resistor's calculated power, which is determined as follows:

(V2 / R) * DutyCycle

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Watt

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.POWER

3007h

02h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2400

1

2400 (0x960)

REGEN.POWER

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.POWER

2400

Unsigned32

Read Only

-