MLFB_DriveFault

Pipe Network motion icon

 Function Block - Returns the fault status, number, and description of the requested axis mapped to a Kollmorgen drive.

  • The FAULT output returns TRUE when the selected drive goes into a fault state.
  • The fault number and description depend on the drive type mapped to the axis.
    • If the drive is an:
      • AKD or AKD2G, the fault number is the same number as reported on the display of the drive.
      • AKT2G Stepper, the fault number represents the drive status word.
        • This word is a bitmask that represents the various error conditions.

Usage

  • Provide drive fault information the application program uses to determine next steps.
    • Example: Perform a machine-controlled stop or perform an immediate disable of the servo drives.
  • In the application program, sends output fault information from this UDFB to the HMI for review by the machine operator.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

EN

BOOL

FALSE, TRUE

N/A

No default

Enables the KollmorgenUDFB.

Used in the FFLD editor only.

AxisID

DINT

-2147483648 to 2147483647

N/A

No default

ID of the axis block of the Pipe Network.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

FAULT

BOOL

FALSE, TRUE

N/A

TRUE if the selected drive currently has a Fault.

FaultNumber

DINT

No range

N/A

If the axis is:

FaultDescription

STRING

N/A

N/A

Description of the fault.

Bitmask Causes

Bit

Description

Cause

0

Saturated

Drive stage operates with maximum duty cycle.

1

Over temperature.

Internal temperature is higher than 80 °C.

2

Torque overload.

Motor current is higher than the rated current.

3

Under voltage.

Motor supply voltage is either:

  • 20% lower than the configured nominal voltage (warning).
  • Less than 8V.

4

Over voltage.

Motor supply voltage is 10% higher than the configured nominal voltage.

5

Short circuit A.

Short circuit in motor coil A.

6

Short circuit B.

Short circuit in motor coil B.

7

No control power.

Control voltage at the power contacts is less than 12V.

8

Misc. error.

Either:

  • The terminal initialization failed.
  • Supply voltage is less than 8V.
  • Internal terminal temperature is higher than 100 °C.

9

Configuration error.

CoE change has not yet been adopted into the current configuration.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Execute and Read the Function Block
Inst_MLFB_DriveFault(PipeNetwork.AXIS1);
Axis1Fault := Inst_MLFB_DriveFault.FAULT;
Axis1FaultNumber := Inst_MLFB_DriveFault.FaultNumber;
Axis1FaultDescription := Inst_MLFB_DriveFault.FaultDescription;

See Also