MLIntInit
Function - Initializes an integrator object.
- The function is automatically called if an Integrator Block is added to the Pipe Network.
- User-defined settings are entered in the Pipe Blocks Properties screen.
- The Integrator object can operate in modulo or not modulo mode.
- While in modulo mode, the output values are adapted according to the entered ModuloPosition value.
Figure 1: MLIntInit
-
-
- Integrator objects are normally created in the Pipe Network using the graphical engine.
- You do not have to add MLIntInit functions to their programs.
- Parameters are entered directly in pop-up windows; the code is automatically added to the current project.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of a created Pipe Block. |
|
ModuloPosition |
LREAL |
No range |
User units |
No default |
|
|
Modulo |
BOOL |
FALSE, TRUE |
N/A |
No default |
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Initiate an Integrator Pipe Block named “MyIntegrator” with a Modulo of 360
MLIntInit(MyIntegrator, 360.0, true );
See Also