Trigger
|
Name |
Description |
|---|---|
|
Clears the flag of an initiated Trigger block. |
|
|
Initializes a Trigger object for use in a PLC program. |
|
|
Checks if the selected block has been triggered. |
|
|
Returns the time the trigger block uses to compensate the delay of the sensor that captures the triggering signal. |
|
|
Returns the position of the block at the moment when it was triggered. |
|
|
Returns the time of the moment where the block was triggered in milliseconds. |
|
|
Sets the edge configuration for a trigger block (e.g., rising, falling, etc.) |
|
|
Sets the time the trigger block uses to compensate for the delay introduced by the sensor that captures the triggering signal. |
Purpose
Computes the local pipe value from the timestamp of a Fast Input time event.
- Pipe input values are passed through to the block output with no influence on the flow of pipe values.
- Typical application is for PLCopen Registration.
Figure 1: Example: Trigger extrapolates output value
There are network and mechanical delays in systems that make capturing a correct pipe position difficult.
To remove the delays, use a sampler block to capture the actual position of an axis.
Figure 2 shows how this works:
Figure 2: Example: Trigger Block
- This sampler block is configured to capture the actual position of axis 1.
- The conversion and axis blocks are only needed to terminate the pipe.
- MLTrigWriteDelay may still be needed to compensate for sensor delay.
- If you need to calculate the master pipe value corresponding to the captured axis position, add the difference between the axis command position and the master pipe value.
Parameters
|
Parameter |
Description |
|---|---|
|
Input_Axis |
Name of the axis where the Fast Input is located. |
|
InputID |
ID number of the Fast Input. Valid values of InputID are:
|
|
TriggerMode / Edge |
The edge to trigger on.
|
Example: Trigger Functions
-
-
- The trigger delay must be calculated by you and set with MLTrigWriteDelay.
- This delay belongs to the sensor.
- It is in addition to the MLTrigReadTime / MLTrigReadPos.
When you call the MLTrigClearFlag function, the flag for trigger is reset to FALSE. (Figure 3)
Figure 3: Example: MLTrigClearFlag = FALSE
When a Fast Input is set, the MLTrigIsTriggered function returns TRUE. (Figure 4)
Figure 4: Example: MLTrigIsTriggered = TRUE
Then call the MLTrigReadPos and MLTrigReadTime functions to get more details. (Figure 5)
Associated Data
- OutputValue: Output value of the data flows.
- TRIG_POS: interpolated position calculated when the time event was triggered (reserved for debugging purposes).
- TRIG_TIME: time when the event was triggered (reserved for debugging purposes).
- DELTA_TRIG_TIME: reserved for debugging purposes.