SetCsvOpt

PLCopen motion icon This function/function block was added in KAS v4.04

 Function - Configures the field separator and decimal point symbol for CSV files generated by the LogFileCSV function block.

  • By default, the LogFileCsv block uses:
    • Semicolons ( ; ) as field separators.
    • Dots ( . ) as decimal points.
    • The SetCsvOpt function to modify these characters to suit specific formatting requirements.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Sep

STRING

Single character.

N/A

;

Defines the field separator (semi-colon) used in CSV files.

Dec

STRING

Single character.

N/A

.

Specifies the decimal point character for numeric values in CSV files.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

BOOL

FALSE, TRUE

N/A

  • Returns TRUE when the function successfully executes.
  • Returns FALSE if inputs are not single character strings.

FBD Language Example

Not available.

FFLD Language Example

IL Language Example

Not available.

ST Language Example

OK := SetCsvOpt(strSeparator, strDecimal);

See Also