REPEAT UNTIL END_REPEAT
Syntax
REPEAT
<statements>
UNTIL <BOOL expression>
END_REPEAT;
Remarks
- The statements between REPEAT and UNTIL are executed until the Boolean expression is TRUE.
- The condition is evaluated after the
statements are executed.
- Statements are executed at least once.
-
-
- Loop instructions can lead to infinite loops that block the target cycle.
- Never test the state of an input in the condition because the input is not refreshed before the next cycle.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
iPos := 0;
REPEAT
MyArray[iPos] := 0;
iNbCleared := iNbCleared + 1;
iPos := iPos + 1;
UNTIL iPos = iMax
END_REPEAT;
See Also