LABELS
Remarks
Labels are used as a destination of a jump instruction in FDB, FFLD, or IL language.
Labels and jumps cannot be used in structured ST Language.
- A label must be represented by a unique name, followed by a colon :.
- In all languages, it is not mandatory that a label is a target of a jump instruction.
- Use label for marking parts of the programs in order to increase its readability.
FBD Language Example
- Labels can be inserted anywhere in the diagram.
- They are connected to nothing.
In this example, the DTAt block is not called if bEnable is TRUE.
FFLD Language Example
- A label must identify a rung.
- It is shown on the left side of the rung.
In Figure 1, Network #6 is skipped if IN1 is TRUE.
IL Language Example
Not available.
ST Language Example
Not available.
See Also