Transition Between Moves

A transition mode must be specified when a new move is appended to a move that is already in progress.

  • Different transition parameters may be required, depending on the transition mode.
  • This characterizes the contour of the transition segment.

The supported transition modes are:

Transition Mode Parameters

Parameters

Number of Transition 
Parameter Array Elements

Transition Parameter Index

Transition Parameter Name

Transition Parameter Description

Units

TM_NONE

0

N/A

N/A

No transition.

N/A

TM_CORNER_DISTANCE

2

0

Corner Distance

Distance to the corner of the deviation and the return point from the original contour.

User units

TM_CORNER_DISTANCE

2

1

Velocity

The velocity value of the transition segment.

User units / sec

TM_SCURVE_CORNER

1

0

Corner Distance

Distance to the corner of the deviation and the return point from the original contour.

User units

No Transition (TM_NONE)

Insert no transition contour segment.

 

Motion Path

 

Motion Velocity Profile

  • The motion blocks are not modified and no transition curve is inserted using this mode.
    • This is the only possible transition mode for the Buffer Modes.
  • No transition parameters are used for this transition mode.

Corner Distance (TM_CORNER_DISTANCE)

Transition with given corner distance.

 

Motion Path

 

Motion Velocity Profile

The corner distance transition mode is specified using TM_CORNER_DISTANCE as the transition mode for a motion block.

Transition Parameter Index

Transition Parameter Index

Name

Description

0

Corner Distance

Distance to the corner of the deviation and the return point from the original contour.

1

Velocity

The velocity value of the transition segment.

  • Corner Distance transitions are handled differently, depending upon whether the connecting moves are lines or arcs, and all of the possible combinations, (line-line, arc-arc, line-arc, arc-line).

S-Curve Corner (TM_SCURVE_CORNER)

Transition with given corner distance, using Jerk for each axis profile.

 

 

Motion Path

 

Motion Velocity Profile

The S-Curve Corner transition mode is specified using TM_SCURVE_CORNER as the transition mode for a motion block.

Transition Parameter Index

Transition Parameter Index

Name

Description

0

Corner Distance

Distance to the corner of the deviation and the return point from the original contour.

  • All S-Curve Corner transitions start and end the transition with zero acceleration.
    • If an S-Curve Corner transition is used with buffer mode BM_ABORTING and during acceleration or deceleration phases of the first move, then the axes experience an acceleration discontinuity at beginning of the transition.
  • Only Line-to-Line transitions are supported with S-Curve Corner.
    • Line-arc, arc-arc, arc-line are not supported.
  • Line-to-Line transitions shorten the next move by the corner distance.
  • Changes to the velocity override during the transition do not take effect until after the transition has completed.
  • S-Curve Corner transitions only depend on the corner distance, the incoming and outgoing move velocities, and the incoming and outgoing move directions.
    • The transition may exceed the maximum specified values for velocity, acceleration, deceleration, and jerk of the incoming and outgoing moves.
      • Jerk and peak acceleration increase with a larger angle between the incoming and outgoing move directions.
      • Jerk and peak acceleration decrease with a larger corner distance.
  • To approximate the path peak acceleration and jerk during the transition, we can use these equations:
    • Vavg = The average of the slew speeds of the incoming and outgoing moves.
    • θ = The angle between incoming and outgoing moves.
    • CD = Corner distance.
    • If actual accel = ka typical accel and actual jerk = kj typical jerk, then:
      • ka has an average value of 1 with a standard deviation of 0.5.
        Values of ka have been observed as large as 3.
      • kj has an average value of 1 with a standard deviation of 1.1.
        Values of kj have been observed as large as 12.

  • The formulas are approximate guidelines.
    Your application may experience different behavior.

See Also