Calling Function Blocks Multiple Times Same Cycle
A given function block can usually be called multiple times without causing problems when using a single-core controller.
Example
It is possible to call MC_MoveVelocity multiple times to start velocity moves on multiple axes.
Set the Execute input to False between every call to start a new velocity move.
- When doing this, the ability to monitor the status of the velocity moves is lost because the axis parameter is changed for each call.
- If there is no concern with monitoring the status of the velocity moves, call MC_MoveVelocity any number of times in a given cycle.
Function blocks that start a motion-related action need to avoid race conditions when using a multi-core controller.
The function blocks have to save argument data so that calculations and error detection can be determined during the next controller cycle.
There are two consequences to this:
- With the possible exception of the multicoreFbExecuteDuplicateValueInCycle error 76, the Error and ErrorID outputs report no error on the first cycle.
- The Error and ErrorID outputs reports their status in the next VM cycle.
- The function block cannot be called with the same Execute state twice in a single VM cycle.
- If a function block is called with the same Execute state twice in a single VM cycle, a multicoreFbExecuteDuplicateValueInCycle error 76 is returned immediately.
Function Blocks - Start Motion-related Actions
See Also