Axis Parameters
Boolean Parameters
This table is a list of Boolean supported parameters.
These parameters are read and written by the function blocks MC_ReadBoolPar and MC_WriteBoolPar.
Parameter Details
|
ID |
Parameter |
Name |
R/W |
Update Rate Type |
Description |
|---|---|---|---|---|---|
|
MC_AXIS_PARAM_IN_POSITION |
Axis In-Position |
Read-only |
|
||
|
MC_AXIS_PARAM_DRIVE_WARNING |
Drive Warning |
Read-only |
Drive Warning Status. See Note 1. |
||
|
MC_AXIS_PARAM_REGIST_GOOD |
Good Registration Mark Occurred |
Read-only |
|
||
|
MC_AXIS_PARAM_REGIST_BAD |
Bad Registration Mark Occurred |
Read-only |
|
||
|
MC_AXIS_PARAM_FI_OCCURRED |
Fast Input Occurred |
Read-only |
Deprecated Behavior
|
||
|
MC_AXIS_PARAM_APPLY_SUPERIMPOSED_DISTANCE |
Apply Superimposed Distance |
Read / Write |
The default value for this parameter is FALSE.
Param 1033 = False
Param 1033 = True Note
|
||
|
MC_AXIS_PARAM_IGNORE_DRIVE_LIM_STATUS |
Ignore Drive Limit Active |
Read / Write |
|
||
|
MC_AXIS_PARAM_DRIVE_OVERRIDE_ON_LIMIT_ACTIVE |
Drive Override on Limit Active |
Read / Write |
|
Notes
See Tuning Controller Performance for EtherCAT Communication Latency.
- This is a configuration parameter.
- There is some delay in acquiring fast input information from drives and calculating the registration marks.
While the information is evaluated cyclically, there may be a few cycles between when the fast input occurs and the system records the registration marks. - There is some delay in acquiring fast input information from drives and calculating the fast input position.
While the information is evaluated cyclically, there may be a few cycles between when the fast input occurs and the system records the fast input data. - There is some delay in acquiring the actual position values.
While the information is evaluated cyclically, there may be a few cycles between when the actual position is updated in the drive and the system records the fast input data.
Non-Boolean Parameters
This table is a list of supported non-Boolean parameters.
These parameters are read and written by the function blocks MC_ReadParam and MC_WriteParam.
|
|
|
|
|
|
|
|
Parameter Details
|
ID |
Parameter |
Name |
R/W |
Update Rate Type |
Description |
|---|---|---|---|---|---|
|
MC_AXIS_PARAM_CMD_POS |
Command Position |
Read-only |
|
||
|
MC_AXIS_PARAM_ACT_VEL |
Actual Velocity |
Read-only |
|
||
|
MC_AXIS_PARAM_CMD_VEL |
Command Velocity |
Read-only |
|
||
|
MC_AXIS_PARAM_PHASE_SHIFT |
Phase Shift |
Read-only |
|
||
|
MC_AXIS_PARAM_SUPERIMPOSED_DISTANCE |
Superimposed Distance |
Read-only |
|
||
|
MC_AXIS_PARAM_MASTER_OFFSET |
Master Offset |
Read / Write |
|
||
|
MC_AXIS_PARAM_SLAVE_OFFSET |
Slave Offset |
Read / Write |
|
||
|
MC_AXIS_PARAM_MOVE_TYPE_ACTIVE |
Active Move Type |
Read-only |
The active move type. See Move Types. |
||
|
MC_AXIS_PARAM_MOVE_TYPE_NEXT |
Next Move Type |
Read-only |
The queued (next) move type. See Move Types. |
||
|
MC_AXIS_PARAM_POSITION_ERROR |
Position Error |
Read-only |
Position error in user units. |
||
|
MC_AXIS_PARAM_FEEDBACK_LAST |
Raw Feedback |
Read-only |
|
||
|
MC_AXIS_PARAM_ROLLOVER_POSITION |
Rollover |
Read / Write |
In particular: {equation}NewPosition = OldPosition * (New Rollover) / (Old Rollover){/equation}.
|
||
|
MC_AXIS_PARAM_VELCOMP_FACTOR |
Velocity Compensation Factor |
Read / Write |
|
||
|
MC_AXIS_PARAM_VELCOMP_FILTER |
Velocity Compensation Filter |
Read / Write |
|
||
|
MC_AXIS_PARAM_IN_POSITION_BAND |
Axis In-Position Bandwidth |
Read / Write |
The bandwidth about the command position to determine the state of the in-position flag. See Note 2. |
||
|
MC_AXIS_PARAM_DRIVE_STATUS |
Drive Status |
Read-only |
|
||
|
MC_AXIS_PARAM_UU_FB_RATIO_NUM |
User Unit to feedback unit ratio numerator |
Read-only |
|
||
|
MC_AXIS_PARAM_TORQUE_ACTUAL |
Actual Torque |
Read-only |
|
||
|
MC_AXIS_PARAM_BUS_ADDRESS |
Drive Address |
Read-only |
|
||
|
MC_AXIS_PARAM_SENSOR_DELAY |
Sensor Delay |
Read / Write |
Compensation for Physical sensor delay for MC_TouchProbe, in microseconds. See Note 1. |
||
|
MC_AXIS_PARAM_INTERP_CMD_POS |
Interpolated Command Position |
Read-only |
|
||
|
MC_AXIS_PARAM_INTERP_CMD_VEL |
Interpolated Command Velocity |
Read-only |
|
||
|
MC_AXIS_PARAM_REGIST_COMP |
Registration Compensation |
Read-only |
|
||
|
MC_AXIS_PARAM_REGIST_DIST |
Distance Between the Last Two Good Registration Marks |
Read-only |
|
||
|
MC_AXIS_PARAM_REGIST_GOOD_CNT |
Number of Consecutive Good Registration Marks |
Read / Write |
|
||
|
MC_AXIS_PARAM_REGIST_BAD_CNT |
Number of Consecutive Bad Registration Marks |
Read / Write |
|
||
|
MC_AXIS_PARAM_UU_FB_RATIO_DEN |
User units to feedback unit ratio denominator |
Read-only |
|
||
|
MC_AXIS_PARAM_CM_ACT_CMD_POS |
Coordinated Motion Applied Command Position |
Read-only |
Amount of motion actually applied to the PLCopen axis drive by Coordinated Motion commands. |
||
|
MC_AXIS_PARAM_CM_CMD_POS |
Coordinated Motion Command Position |
Read-only |
Amount of motion requested of a PLCopen axis by the Coordinated Motion commands. |
||
|
MC_AXIS_PARAM_INGEAR_BANDWIDTH |
In Gear bandwidth |
Read / Write |
|||
|
MC_AXIS_PARAM_DRIVE_AXIS_NUMBER |
Drive Axis Number |
Read-only |
One-based number that specifies the axis on the drive. |
||
|
MC_AXIS_PARAM_UU_FB_RATIO |
User units to feedback unit ratio |
Read-only |
|
||
|
MC_AXIS_PARAM_BUS_INTERFACE_TYPE |
Bus Interface Type |
Read-only |
The parameter value is:
|
||
|
MC_AXIS_PARAM_SIM_CLOSING |
Simulator Distance Closing Fraction |
Write-only |
This setting affects how responsive a simulated axis to changing command positions.
Values are broken down into these ranges:
|
||
|
MC_AXIS_PARAM_UU_REV_RATIO |
User units revolution ratio |
Read / Write |
|
||
|
MC_AXIS_PARAM_BUS_POSITION_DEMAND |
Position demand value |
Read-only |
Drive Position Demand Value 32-bits.
|
||
|
MC_AXIS_PARAM_BUS_STATUS_WORD |
Drive Status Word |
Read-only |
Drive Axis Status Word 16-bits.
|
||
|
MC_AXIS_PARAM_BUS_CONTROL_WORD |
Drive Control Word |
Read-only |
Drive Axis Control Word 16-bits.
|
Notes
See Tuning Controller Performance for EtherCAT Communication Latency.
- This is a configuration parameter.
- There is some delay in acquiring fast input information from drives and calculating the registration marks.
While the information is evaluated cyclically, there may be a few cycles between when the fast input occurs and the system records the registration marks. - There is some delay in acquiring fast input information from drives and calculating the fast input position.
While the information is evaluated cyclically, there may be a few cycles between when the fast input occurs and the system records the fast input data. - There is some delay in acquiring the actual position values.
While the information is evaluated cyclically, there may be a few cycles between when the actual position is updated in the drive and the system records the fast input data.
Update Rate Types
Controller
The update rate depends on KAS application program update rate.
See Define the PLC Cycle.
EtherCAT Cyclic
The update rate depends on the EtherCAT.
See these topics about update rates:
EtherCAT Non-Cyclic
The update rate depends on the reading of the parameter through EtherCAT.
Static
- If read-only, the values do not change after the axis is created.
- If read / write, the values change only when the user sets the value.
User Units to Feedback Units Ratio
Parameters Non-Boolean Parameters and Non-Boolean Parameters are set during the MC_CreatePLCAxis function block execution.
- These two parameters work together to form the User Units to Feedback Units Ratio (UU/FBU Ratio).
- The drive interface units are fixed by the drive and define the drive units per revolution.
- This is used to command the drive per the ratio.
Example 1
Where the drive interface units are set to 1048576 units per revolution, the value of the UU-per-revolution ratio is calculated as:
UU per revolution = MC_AXIS_PARAM_UU_FB_RATIO_NUM * 1048576 / MC_AXIS_PARAM_UU_FB_RATIO_DEN
Example 2
A Drive with a Ratio of:
Generates
Revolution of Drive Motor
Generates
UU-to-FBU Ration
360 UU / 1048576 FBU
360 UU
0.000343323
11379 UU / 1898996404 FBU
6.283185 UU
5.99211e-6
Example 3 - Reading the Current to Units of Amps
After reading the current using MC_ReadParam, this equation converts current to amps for a 12 amp peak drive:
MC_AXIS_PARAM_TORQUE_ACTUAL * Drive Continuous Current Rating / 1000