Map Input and Output to Variables
I/O from the EtherCAT motion bus or the controller is easily mapped to PLC variables through the Project Explorer.
The exact process varies slightly depending on the device.
- Expand the Controller, and EtherCAT nodes in the Project tree.
- Double-click on the device or I/O slice entry.
- Map the variables in any of three ways:
- Drag and drop variables from the Dictionary.
- Use the PLC Variable Creation Wizard for Kollmorgen devices.
- Directly map / unmap the inputs and outputs using the PLC Variable Selector dialog box.