EtherCAT Devices tab

The EtherCAT Devices tab lists all the EtherCAT devices and provides the ability to discover and map their use. (Figure 1)

  • The interface is slightly different for AKD and AKD2G drives.
  • The AKD2G prompts you to select the mapping by the drive axis.

EtherCAT Summary Form

Figure 1: EtherCAT Devices Summary Form


  • First generation AKDs and Kollmorgen Essentials Drive support one axis per drive.
    AKD2G drives support two axes per drive.
    When configuring drives in the EtherCAT Devices tab, you must designate which motion axis applies to each drive axis, which is the actual axis the drive controls.

EtherCAT Devices

Item

Description

Show only drives

This option hides all EtherCAT slaves from the list that are not drives.

Scan Devices

The KAS Runtime sends EtherCAT messages to discover the physical devices and modules present in the network.

See Scan Devices.

Name, Vendor, Product, and Model

  • The project device name, vendor name, product name (or code number), and model number for each device is displayed and ordered by the position in the tree.
  • The model (when available) includes the extension and connectivity options (e.g., NBEC).
  • See AKD Models and AKD2G Model Description about interpreting the model text of Kollmorgen drives.

FW Version

  • For Kollmorgen drives, the firmware version is displayed on the conditions that: 
    • The Scan Devices routine was run successfully on the EtherCAT network (for drives with version 01-08-000-00 firmware or later).
    • Firmware was downloaded to the drive(s) while the KAS project was open in the KAS-IDE.
  • For other devices, the firmware version appears if the Scan Devices routine was successfully run and the device supports reading this information over EtherCAT (i.e., it uses CoE object 0x100A:0).
  • Otherwise (Unknown) is displayed.

    • If a Kollmorgen drive is showing the firmware version as Unknown, the drive has valid resident firmware (to boot from), but does not have valid operational firmware.
    • Download and install the latest operational firmware and reboot the AKD / AKD2G.

Drive Axis Number

  • This number designates which axis, of those available on a drive, is being defined.
  • For most drives, this number is a 1.
  • For AKD2Gs, there are two entries:
    • Drive Axis Number 1.
    • Drive Axis Number 2.

Mapped to Axis

For each drive, it is displayed if it is:

  • Unassigned: From the drop-down menu, choose an axis that has not been assigned.
    • It is applicable for either PLCopen or Pipe Network motion engines.
  • Already mapped to a physical device: The mapping operation is done using the Scan Devices command.
  • If a drive node is removed from the EtherCAT network using ECATDeviceAction, then the mapped axis (if any) is automatically forced to simulation.

Simulated

Used to simulate the device, which means that the device is not used and no communication to this device is performed through the fieldbus.

When can drives can be simulated?

Mapped to an Axis?

Simulated State

No

Simulation is not applicable

Yes

  • If the Drive is mapped to a physical drive, then the simulation is Enabled.
    • Set the state to Yes/No --> Display check box.
  • If Drive is not mapped to a physical drive, the Simulation is forced to Yes.

Save parameters to NV memory

  • Save the drives' parameters to the NVRAM of each drive currently selected in the list.
    • This action is enabled only when the Online Mode is activated.
  • You are automatically prompted to save modified drive parameters if this action has not been performed prior to these circumstances:

Upgrade Firmware

  • This command triggers a firmware upgrade for the selected drives.
  • Use Ctrl+A shortcut to select all drives.
  • For more details, see the FAQ Setup section.

Scan Devices

The scan process allows these tasks:

Figure 2: EtherCAT Network - Physical View

EtherCAT Network - Logical View

EtherCAT Network - Logical View

Figure 3: K-Bus

 

Figure 4: E-Bus

During the scan operation, all physical devices connected to the EtherCAT network are discovered and identified.

  • The KAS-IDE lists the devices in the order they are connected.
  • Kollmorgen devices (e.g., AKD and S300 / S700 drives, Standard I/O Couplers, and remote I/O terminals) include detailed information for each device.

EtherCAT Device Icons

The status of devices can be determined by their icon in the logical view.

Icon

Meaning

Description

(device icon)

Normal

  • The device has been added by scanning the system.
  • The associated ESI file has been found.
  • The icon varies by device, but is the icon set by the manufacturer in the ESI file.

Excluded

The device has been added manually or has been disassociated from a discovered device.

ESI missing

The ESI file is missing.

Error

For AKD, shown when there is an error.

Scan Limitations

  • I/O slices for Standard I/O Coupler do not reveal their Device IDs.
  • The discovery feature does not differentiate between:
    • AKT-DN-004-000 and AKT-DNH-004-000 I/O terminals.
    • AKT-DN-008-000 and AKT-DNH-008-000.
  • Devices other than those made by Kollmorgen are identified by the Vendor Name (or ID number) and Product Name (or ID number).
    • If the device is missing an ESI file, the ESI file supplied by the device Vendor must be imported.
    • The ESI file is required by the KAS-IDE to decode and display the Product Name, Device Description, and other details.
  • ESI files for any MDP devices connected to the network should be added to the KAS-IDE ESI library before starting a scan.
    • If the ESI file for an MDP device is not available, the scan cannot identify the device and cannot discover any physical or logical modules under the device.

Concept Link IconSee Also