Map I/O from the Project Explorer

  1. In the Project Explorer, expand the Controller node and the EtherCAT nodes to access the devices.
  2. Figure 1: AKT (K-Bus) devices

     

    Figure 2: AKT2G (E-Bus) devices

  3. Accessing the device properties is slightly different depending upon the device.
    See Access to Device Properties.
  4. Map the variables:
  5. Select the channels to map.
    Selection may be done by click-dragging or shift-clicking a range of entries.
    The entire table may be selected by clicking on its border.
  6. After the selection is made, right-click and select Map or press <Enter>. (Figure 3)
    This opens the PLC Variable Selector dialog box.
  7. Figure 3: Map or Unmap options


    • The Unmap command in the contextual menu is used to remove the link between the variable and the associated channels.
      Deleting a variable from the dictionary which is mapped to the channels also removes the links.
  8. Choose the variable to link to the channels or PDO object. (Figure 4)
  9. Figure 4: PLC Variable Selector dialog box


    • The list of variables is filtered to display only those with relevant types.

      • Mapping to variables within a structure instance is supported.
      • Mapping to array variables and array variables in a structure instance is supported.
      • Variables assigned to the Safe Digital Input and Safe Digital Output channels must be Read-only.


  • The limitations of PLC variable mapping are:

    • Each PLC variable can be mapped to an EtherCAT I/O and exclusively to either:
      • A Controller Onboard I/O.
      • An external driver.
    • Because a variable can only be mapped to one channel or PDO object, when you link a variable to a new channel or PDO object, the previous mapping is removed (even if linked to another slice or device).
    • Individual bits within a variable can be mapped to multiple I/O channels on different devices (e.g., AKD, PCMM2G, or Slice).

    Example: The same PLC variable cannot be mapped to both PROFINET and a Controller Onboard I/O but it is possible with a regular EtherCAT I/O.

Access to Device Properties

Kollmorgen AKD Series Servo Drives

This includes Kollmorgen Essentials Drive, AKD, and AKD2G.

In the project tree, double-click the drive and select the I/O tab. (Figure 6)

Figure 6: Example: AKD, AKD2G, or Kollmorgen Essentials Drive

KAS Controllers

In the project tree, double-click Controller Onboard I/O in the project tree. (Figure 7)

Figure 7: Example: Controller Onboard I/O

I/O Slice

In the project tree, double-click the I/O Slice under EtherCAT (e.g., AKT2G) or the Coupler entry (e.g., AKT) and click the I/O tab. (Figure 8)

 

For Slice Analog I/O and thermocouples, the offset and gain parameters must be defined. (Figure 9)

Figure 8: E-Bus Properties

Figure 9: K-Bus

Safety I/O Slice

In the project tree, double-click the Safety I/O Slice under EtherCAT (E-Bus) and click the I/O tab. (Figure 10)

Figure 10: E-Bus Safety

See Also