Export the Oscilloscope Data
This procedure exports the trace data to a CSV file.
- Navigate to the Soft Oscilloscope.
- Start the data collection.
- Wait for the probe data to save to be collected.
- Stop the data collection.
- Click the Export... button.
- Select the location where to save the CSV file.
- Click the Save button.
-
-
- The Export operation is possible even when acquisition of samples is in progress.
- When this happens, the latest exported data are the data collected when the CSV file is defined.
- The acquisition of samples is limited to 200 sec when the cycle time is set to 1000 µs (respectively 50 s with 500 µs, and 25 s with 250 µs).
- The Export operation is possible even when acquisition of samples is in progress.