AOUT.VALUEU

Description

AOUT.VALUEU reads/writes the analog output value when AOUT.MODE = 0 (analog output signal is determined by the user).

General Information

Type

R/W Parameter

Units

V

Range

–10 to +10 V

Default Value

0

Data Type

Float

Start Version

M_01-00-00-000

Variants Supported

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex

3470h/3

Related Topics

Analog Output