IL.FF

Description

IL.FF reads the present current loop overall feed-forward value. It is the sum of the following feed-forward paths:

  • Acceleration feed-forward (determined by IL.KACCFF)
  • Velocity feed-forward (determined by VL.KVFF)
  • Friction feed-forward (determined by IL.FRICTION)
  • Gravity offset feed-forward (determined by IL.OFFSET)
  • Bus network feed-forward (determined by IL.BUSFF)

IL.FF is calculated using the following variables' values at the time it is called:

IL.FF = IL.KACCFF * Accelration Command + VL.KVFF * Velocity Command + IL.FRICTION (if motion is currently commanded) + IL.OFFSET (always) + IL.KBUSFF * IL.BUSFF (if fieldbus connected)

For EtherCAT

IL.BUSFF is the injected current feedforward, which corresponds to Object 60B2h: Torque Offset. The scaling for the torque offset is done with 1/1000 rated torque. In AKD, a value of 1000 means DRV.ICONT will be commanded in IL.BUSFF (if IL.KBUSFF is set to 1).

IL.KBUSSFF is a gain setting for the feedforward value IL.BUSFF. It needs to be set to greater zero to let IL.BUSFF take effect. IL.KBUSFF can be access by SDO object 50E2h /0.

The IL.BUSFF gain can be commanded through EtherCAT in all DS402 operating modes.

General Information

Type

R/O Parameter

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

See Also

IL.KBUSFF, IL.KVFF, IL.OFFSET, IL.FRICTION, IL.KACCFF

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes

Related Topics

Current Loop