IL.MFOLDT

Description

IL.MFOLDT sets the time constant of the exponential drop (foldback) of the current towards motor continuous current.

General Information

Type

R/O Parameter

Units

s

Range

0.1 to 2,400 s

Default Value

10 s

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes

Related Topics

Current Loop