MOTOR.KE

Description

MOTOR.KE defines the back EMF constant for the motor. The back EMF constant defines how much voltage is generated at the motors coils. The relationship between MOTOR.KE and speed is described by the following equation:

Coil Voltage = MOTOR.KE * VL.FB

VL.FB is in units of krpm for rotary motors and in units of m/s for linear motors.

The maximum speed for interior permanent magnet motors (IPM) is determined by MOTOR.KE and VBUS.VALUE. An overspeed fault is generated if MOTOR.TYPE is set to 6 (IPM) and VL.FB * MOTOR.KE exceeds VBUS.VALUE.

General Information

Type

NV Parameter

Units

Vpeak/krpm for Rotary Motors

Vpeak/m/s for Linear Motors

Range

0.0 to 100,000

Default Value

0

Data Type

Float

See Also

N/A

Start Version

M_01-03-06-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5260h /0

M_01-03-06-000

Related Topics

Motor View | VL.FB | VBUS.VALUE