MOTOR.TEMPC

Description

When the motor has a thermistor with linear characteristics (MOTOR.RTYPE = 2, 3 or 4), MOTOR.TEMPC returns the motor temperature in degrees Celsius, which is calculated from the resistance of the motor thermistor.

There is no algorithm to convert from resistance to degrees Celsius for non-linear thermistors. In this case, MOTOR.TEMPC returns -32,768 which is an invalid temperature.

General Information

Type

R/O Parameter

Units

Degrees Celsius

Range

-215 to 215

Default Value

N/A

Data Type

Integer

Start Version

M_01-10-04-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3458h/0 M_01-10-04-000

Related Topics

"Motor View" | MOTOR.TEMP | MOTOR.RTYPE