VL.BUSFF

Description

Displays the velocity loop feedforward value injected by the fieldbus. Only active in position mode.

General Information

Type

R/O Parameter

Units

Depends on UNIT.VROTARY (pg 1) or UNIT.VLINEAR (pg 1)

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

Range

0.0 to VL.LIMITP

Default Value

0.0

Data Type

Float

See Also

VL.FF, VL.KBUSFF

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
60B1h/0 M_01-00-00-000

Related Topics

"Velocity Loop"