FB#.ENCLINES

Description

Used to configure the number of lines per revolution for rotary encoders. This keyword is only valid for Incremental and Sin/Cos encoders and is ignored for any other encoders and linear motors.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Lines/revolution

Range

0 to 4,294,967,288

Default Value

1024

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB2.ENCLINES

3501h

02h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30081

1

30081 (0x7581)

FB2.ENCLINES

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB2.ENCLINES

30081

Unsigned32

Read/Write

-