FB#.SSITYPE

Description

FB#.SSITYPE sets the type of SSI device used for position feedbacks. The SSI protocol is flexible and compatible with different feedback models using different implementations. The protocols may differ in the data format of the serial position bits. They also may contain special configuration and flag bits.

FB#.SSITYPE is used when FB#.SELECT = 36 (SSI). It is ignored for other values of FB#.SELECT.

The following table lists the supported SSI types with protocol details and example manufacturers and models.


If the SSI encoder being used does not align with one of the options in the table below, Contact Kollmorgen Customer Support.

Value Protocol Known Models Notes
0

Binary Single- and Multi-turn position bits only


Encoder may use any combination of Single- and Mult-turn bits

Netzer DS-25-SF-S0
1

Gray Code Single- and Multi-turn position bits only


Encoder may use any combination of Single- and Mult-turn bits

Hengstler AD34/1217AF.0NSC0:5942
Baumer EN580E.ML-SU06.G$$1G.13120.H/11250119
2

Special Device - Gurley
1 status bit

Grey code position bits

3 flag bits

1 zero bit

Gurley VP12S08A2CN ‘Initializing move’ required before position values from FB#.P are valid and will cause position jump on completion. See encoder datasheet for details.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-06-03-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.SSITYPE

3500h

12h

Unsigned8

-

-

Read/Write

No

FB2.SSITYPE

3501h

12h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30560

1

30560 (0x7760)

FB1.SSITYPE

Unsigned8

Read/Write

Yes

30561

1

30561 (0x7761)

FB2.SSITYPE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.SSITYPE

30560

Unsigned8

Read/Write

-

FB2.SSITYPE

30561

Unsigned8

Read/Write

-