FFLD Jumps and RETURN
- In the FFLD Language, the >> symbol (followed by the target label name) is used as a coil at the end of a rung. (Figure 1)
- The jump is
performed only if the rung state on input is TRUE.
- The destination label must be specified on a network of the same program.
- To specify the destination, double-click the cell to display a drop-down menu that lists all the available labels.
-
-
The special <RETURN> destination specifies a jump to the end of the program.