Recipes
This
It is intended for:
- Machine builders (OEMs).
- System integrators and distributors.
- Controls Engineers.
- End users and operators.
Recipes enable efficient handling of machine configuration data for different products, improving flexibility, consistency, and traceability.
What is a Recipe?
In industrial automation, a recipe is a named collection of parameter values that together define the configuration for a particular manufacturing process or product variant, sometimes referred to as a SKU.
Rather than hard-coding process parameters into the control program itself, recipes allow operators and engineers to separate what the machine does (the program logic) from how it is configured for a given job (the data).
For a PLCopen-based controller, a recipe file is:
- A structured data set that provides motion-related parameters (e.g., process values and kinematic parameters).
- Loaded at runtime and applied by PLCopen motion function blocks.
An application control logic can remain unchanged while a recipe dynamically configures how machine behavior and motion profiles are executed for a specific product or operation.
Recipes are a foundational concept in batch and discrete manufacturing and are formally described in the ISA-88 (IEC 61512) standard for batch process control.
See ISA-88 Series of Standards.
What Problems Do Recipes Solve?
Modern manufacturing lines frequently produce multiple product variants on the same equipment. Without recipe management, engineers face a difficult choice:
- Hard-code all variants into the program - resulting in complex, branching logic that is difficult to maintain and error-prone to modify.
- Manually adjust parameters at the HMI or in the source code - a slow, undocumented, and risky process that depends entirely on operator knowledge.
Recipe management eliminates both of these problems by providing a structured, systematic mechanism for storing and applying process parameters.
|
Problem |
How Recipes Help |
|---|---|
|
Product changeovers are slow. |
A single operator action loads a complete parameter set instantly. |
|
Parameter changes are undocumented. |
Recipe files are named, versioned, and stored in a traceable format. |
|
Operators can enter invalid values. |
Recipe variables carry type information and can enforce validation limits. |
|
Process knowledge is not documented. |
Parameters are captured in files that can be backed up, shared, and audited. |
|
Scaling to new variants requires code changes. |
A new recipe file is created with no changes to the control program. |
Example Use Cases
|
Example Industry |
Use Case |
|---|---|
|
Food and Beverage |
Switching between product formulations (e.g., flavors, concentrations). |
|
Pharmaceuticals |
Batch manufacturing with strict parameter traceability requirements. |
|
Labeling |
Store label offset, print speed, and dispense timing for different container sizes. |
|
Agricultural Automation |
Define dryer temperature, airflow, and target moisture content for different grain types (e.g., corn, soybeans, wheat). |
|
Laser Notching / Cutting |
Define laser power, pulse frequency, cutting speed, and focus offset for different parts. |