SFC Toolbar
- Items are always inserted before the selected item.
- The chart is automatically re-arranged when a new item is inserted.
Use these keyboard commands when an item is selected:
- ENTER: Edit Level 2 of a step or transition.
- Ctrl+ENTER: Change the number of a step, transition, or jump.
|
Toolbar Button |
Description |
|---|---|
|
Initial step (I) |
Inserts an initial step. |
|
Step (S) |
Inserts a step. |
|
Transition (T) |
Inserts a transition. |
|
Set Timer on Transition |
Sets a timer on a transition. Example: 5 on step number 4 leads to a transition with GS4.T>T#5ms. |
|
Jump (J) |
Inserts a jump to a step. |
|
Divergence (X) |
Inserts the main (left side) corner of a divergence or convergence. |
|
Divergence (D) |
Inserts a divergence corner. |
|
Convergence (C) |
Inserts a convergence corner. |
|
Insert Comment |
Inserts a comment. |
|
Change Display |
Swaps between possible overviews of level 2 in the level 1 chart:
|
|
Swap Item Style |
Allows changes to the item style. Changes either:
|
|
Renumber |
Renumbers all steps and transitions. Previously, the window showing the content of a step or a transition must be closed. |
|
Edit Reference |
Edits the number of a step, transition or jump. Previously, the window showing the content of a step or a transition must be closed. |
|
Show one qualifier in level 2 |
Shows one level of the edition in the level 2 of the SFC Editor. Example: Shows only the P1 of a step. |
|
Show/Hide split window in level 2 |
Shows two levels of the edition in the level 2 of the SFC Editor. Example: Show P1 and Notes of a step. |
|
Show all qualifiers in level 2 |
Shows every level of the level 2 on the SFC Editor. |
Edition window
Open the Edition window using a click on ENTER, when an item is selected.
- The level 2 of a step or a transition can be edited in this window.
- The different levels of editions in the level 2 of the SFC Editor can be selected using the buttons at the top of the Edition window.
|
Toolbar Button |
Description |
|---|---|
|
Action |
Shows/hides the action box in the SFC level 2. |
|
P1 |
Shows/hides the P1 box in the SFC level 2. |
|
N |
Shows/hides the N box in the SFC level 2. |
|
0 |
Shows/hides the P0 box in the SFC level 2. |
|
Notes |
Shows/hides the Notes box in the SFC level 2. |
|
Close level 2 |
Closes the SFC level 2. |