Abort_connection_option_code
| Index.Sub | |
| Data Type | Integer16 |
| Access | Read/Write |
| PDO Mappable |
No |
| Unit | -- |
| Range |
0 = No action 1 = Fault signal 2 = Disable voltage command 3 = Quick stop command |
| Default Value | 0 |
| Store Supported | Yes |
| Description | This object defines the reaction to be executed when a communication abort event is triggered. |
| Notes | -- |