| Default Value |
0 (BiSS Encoder disabled) |
| Description |
This object contains the configuration for the BiSS Encoder. For the correct reading of the BiSS Encoder connected to the drive it is necessary to specify the right resolution (# of bits of either single turn or multiturn). For instance, if the connected BiSS Encoder has a resolution of 17 bits single turn and 16 bits multiturn, The BiSS_Encoder_Config object must be set equal to 4113 (1011H).
|
Byte 3
|
Byte 2
|
Byte 1
|
Byte 0
|
|
Reserved
|
Reserved
|
Multiturn Bits #
|
SingleTurn Bits #
|
|
|
Notes
|
|